2015-07-10 08:06 PM
Hi, been using STM32CubeMX for creating code for ''System Workbench for STM32''. The linker file created by STM32CubeMX has 0 for heap and stack:
_Min_Heap_Size = 0; /* required amount of heap */ _Min_Stack_Size = 0; /* required amount of stack */ I am using latest V1.2.0. The chip is STM32L151RCTx. If I look at the linker files in the ''../Templates/gcc/linker'' folder of STM32CubeMX, they all have 0x200 heap size and 0x400 stack size. Not sure why the linker file in created code has 0. Think it should be 0x200 and 0x400 for linker file of created code too. #stm32cubemx-stm32l1-linker2015-07-17 07:34 AM
You are correct. The bug has been raised to be fixed in next MX release.
Best regards2015-12-01 03:38 AM
Dear user,
Please note this issue is now solved.