2024-03-30 06:45 PM
I'm using the STM32H573I-DK and it works great. We are running the Fx_uSD_File_Edit example. We are creating a product that leverages a lot of the dev kit design, but we want to use eMMC instead of SD card. I took the Fx_uSD_File_Edit example ioc and altered SDMMC1 to be "MMC 4 bit wide bus". But now FileX does not let me choose "MMC interface". I tried quitting out of STM32CubeMX and restarting it. No help. I disabled SDMM1 and re-enabled "MMC 4 bit wide bus". FileX MMC interface is still greyed out. What can I do to change to MMC for FileX? I've attached my .ioc
BTW, I have another unrelated STM32U5 project and I can choose FileX MMC interface there. Why not in STM32H5?
2024-04-02 06:28 AM
hello @billw
I confirm the issue and it is reported internally.
Internal ticket number: 178050 (This is an internal tracking number and is not accessible or usable by customers).
With Regards
Kholdoun