2014-08-07 1:42 PM
STM32CubeMX ver.4.3.0 / STM32Cube V1.0
Generated the attached STM32CubeMX project file.Upon reloading the project the Clock Configuration tab is empty - it does not show the clock tree info.What should I do to fix the Clock Configuration tab in order to show the clock tree? #stm32cubemx-clock-configuration2014-08-08 6:16 AM
Hello Adim,
Thanks for the feedback. We confirm that there is a bug when loading this .ioc. In fact, the problem is encountred when loading the RCC.HSE_VALUE that contains ''.3''. As workArownd to be able to load correctly this configuration and to have the Clock Configuration tab, you can just modify this line ''RCC.HSE_VALUE=4524583.3'' by ''RCC.HSE_VALUE=4524583''. This issue will be fixed in the next release ''v4.4.0''. Best regards, Amel.