cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMx does not show available templates in Template Settings

themole
Associate II

Hello,

I'd like to use the user template settings (CubeMX Project -> Project Manager -> Code Generator -> Template Settings) to add own files to the generated project, but unfortunately, it neither shows available templates from the (default) extra_templates folder, nor from any other folder I select. There are definitely ftl files located in the extra_templates folder (see attached screenshot)

Regards,

Daniel

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
ECata.2
Associate

Hi,

I have the same issue.

Did you got a solution?

Best regards

CGemb.1
Associate II

I got around this by:

  1. selecting a custom template folder.
  2. re-select the original folder