2022-11-30 08:17 AM
We are pleased to announce you that the official release of STM32CubeMX v6.7.0 is available for download here
What is new in STM32CubeMX V6.7.0?
Main fixed issues
130537 [Project Manager] Wrong call order for MDMA/DMA Init functions
119809 [MX-L5][CodeGen] Warning generated when IP initialization as a pair of .c/.h
125698 [Cortex-M7] No default MPU configuration is proposed
126668 [MX-HRTIM][LL] Issue in HRTIM init in LL code when "General peripheral initialization as a pair of .c/.h files per peripheral " parameter is checked
128892 [IDE-GUI][H7]Changing MDMA list type from linear to loop listing causes MX tab to appear * even after saving modification
131802 [MX-CodeGen][H7] Project showing error during generation after enabling multi-threaded support checkbox for cortexM7
132093 [DMA] MX_DMA_Init() is called after MX_TIM23_Init()
133163 [STM32CubeMx] [DRR] DDR3 settings unavailable using STM32CubeMX
134921 [HRTIM] HRTIM generated code that enable Resynchronized Update even we disable it
134934 Execution in RDP-2 impacted by DWT-based code in SystemClock_Config()
135590 [MX-ETH][MW-LWIP] HAL_ETH_Start should be replaced with HAL_ETH_Start_IT in "ethernet_link_thread" function
137342 [STM32CubeMx] [FreeRtos] The tool can't open the *.ioc file if user constants are used with FreeRtos
138331 Issues with toolchain location folder and Makefile toolchain
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-01 12:33 AM
It looks like CubeMX 6.7 with DB 6.0.70 does not create the Freertos Task creation calls anymore.
First picture, DB-6.0.60 - Calls beeing created.
With CubeMX 6.7 and DB6.0.70 a new Fileheader is being created an no calls to create any Tasks / Queues / Mutexes etc.
Steps to reproduce:
Create new Project with CubeMX (STM32F407 in my case), Add FreeRTOS, Save & Generate ->
No call to osTheadNew for the default task will be created.
2022-12-01 05:16 AM
I can‘t generate freertos task creation with CMSIS v2 either. And I find cubemx can generate successfully with cmsis v1. It's a bug.
2022-12-01 10:11 AM
> 134934 Execution in RDP-2 impacted by DWT-based code in SystemClock_Config()
Is DWT disabled in RDP2 state? Not just the debugger connection is blocked?
2022-12-04 07:12 AM
1 more error. This version is currently unusable
LWIP
identifier "ETH_RX_BUFFER_SIZE" is undefined
2022-12-04 10:48 AM
I have reported this some days ago.
And found the bug inside the FREERTOS-STM32F4xx_Configs.xml file.
Search for my question "What happens to FreeRTOS code generation" to see how to fix it.
2023-01-10 11:29 AM
(removed and reposted elsewhere)
2023-01-11 12:00 AM
Hello @Lars Beiderbecke
First let me thank you for posting and just say that it's recommended that you post your question as a separate poste on the forum to make it easier to be found by other community members
Concerning the issue you are facing could you please provide more details:
Waiting for your feedback.
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-13 06:29 AM
Of course, will do!
Regards
Lars
2023-01-21 07:58 AM
hello! When I started install CubeMX, I have error: ---------------------------
Java Virtual Machine Launcher
---------------------------
Error: A JNI error has occurred, please check your installation and try again
---------------------------
OK
---------------------------
and also the next error:
---------------------------
Java Virtual Machine Launcher
---------------------------
A Java Exception has occurred.
---------------------------
OK
---------------------------
how to solve these errors?