2021-09-16 7:08 AM
Hi,
i'm using Keil with the ARMClang 6.x compiler, an STM32f407 and CubeMX to configure my project.
I was playing arround with dynamic memory allocation and was wondering why
uint8_t* b_;
b_ = static_cast<uint8_t*>(std::calloc(100, sizeof(uint8_t)));works but
b_ = static_cast<uint8_t*>(std::calloc(512, sizeof(uint8_t)));always was returning 0x0000000.
After reading on the ARM/Keil website i came to the conclusion that
IMPORT __use_two_region_memoryin the startup_stm32f407xx.s seems to be the reason for this fault(?)
I'm not exactly sure if this is a fault or to be excpected and i'm overseeing sth. But after comenting out this line i get a valid pointer when i try to allocate 512 byte (or more)
Why is it working i if allocate a smaller memory area?
And can i fix this somehow so that not everytime i generate the project again my startup file is overwritten? Or is this something which should be fixed in this startup file by ST?
Thanks for help.
2021-09-16 8:49 AM
>>Why is it working i if allocate a smaller memory area?
How much HEAP have you specified?
2021-09-16 9:43 AM
Btw: i'm using c++ so i cannot use the microlib which seems to have an impact on this (some lines before it is taken care of)
I did not change the standard 0x200 defined in this file.
I tried to allocate 500byte(did not work), 256byte did work.
When i comment out the __use_two_region_memory line it is always working (1kb is no problem)
But at the moment i'm asking myself why i can allocate 1kb when i define only 0x200 Byte of heapspace. I did not Touch this low level stuff before so i think i have to get more knowlledge
2021-09-16 10:17 AM
And i use rtx5. I hope it does not configure sth in the back which has impact on this behaviour