cancel
Showing results for 
Search instead for 
Did you mean: 

software problem after and before update CubeMX and IDE

Ali10
Associate
software problem after and before update CubeMX and IDE

hi there

could you help me with this;

after updating CUBMX to latest one 6.14.1, does not open the project automatically , even when i open it from IDE with existing project from CUB MX option , still comes up with this error ;

 

This file has been generated with STM32CubeMX version '6.14.1'.Your current STM32CubeMX version is '6.4.0'.
Please check for update: Help > Check for Updates

 

THE FUNNY THING IS THE LATEST UPDATE FOR CUB MX IS 6.14.1 SO WHY DETECTS THE VERSION WRONG, WHICH IS NOT EXIST ( 6.4)!?

 

SO I CAN NO LUNCH PROJECT FROM CUB MX TO IDE either. 

 

could you help me with this?

 

regards

Ali10

2 REPLIES 2
TDK
Super User

STM32CubeIDE has a bundled STM32CubeMX version. When you open an IOC from within STM32CubeIDE, it uses this bundled version. The only way to update the bundled STM32CubeMX it is to update STM32CubeIDE itself. You can either do that or you can leave it as-is and use the standalone STM32CubeMX to open it. Either way works.

If you feel a post has answered your question, please click "Accept as Solution".
Peter BENSCH
ST Employee

@Ali10 Well... from STM32CubeIDE 2.0 everything will be better and hopefully clearer.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.