2020-03-13 8:49 AM
When using SAI for I2S, STM32CubeIDE does not give you the option to choose Mono mode. It's only option is Stereo Mode. However, STM32 SAI HAL supports both SAI_STEREOMODE as well as SAI_MONOMODE, so I think this should be an option.
2021-12-14 6:39 PM
Hello I am using STM32F407 discovery kit, CubeIDE 1.8.0 and FW_F4 V1.26.2.
I plan to connect the mono mic via I2S as well and should be connected in mono mode.
Where do you get to change hsai_BlockA1.Init.MonoStereoMode to mono mode?
I cannot seem to find this code.
I am looking in:
MX_I2S2_Init(),
stm32f4xx_hal_i2s.h,
stm32f4xx_hal_i2s_ex.h, and
stm32f4xx_hal_i2s.c.
Where should I look for to modify?
2021-12-14 11:07 PM
This thread discusses SAI module, which is not present in the 'F407.
The SPI/I2S module does not have MONO option.
JW
2021-12-14 11:41 PM
Sorry, my bad, just realized that!
Anyway, "The SPI/I2S module does not have MONO option"
can I use?
hi2s2.Init.DataFormat = I2S_DATAFORMAT_16B_EXTENDED;
2021-12-15 2:04 AM
I don't know. I don't know your application and I don't use Cube.
JW
2021-12-15 2:33 AM
I was using the F411 for mono replay, mono source (for compact size) to mono amplifier - I had to make the data look like stereo to use the HAL driver.