2023-07-31 5:41 AM
Hello,
I am using STM32CubeIDE version 1.13.0 together with STM32CubeMX version 6.9.0-RC9 and the STM32F746IGT6 microcontroller.
I am trying to use TIM2 as a 4 channel Input capture unit, each channel with it's own independent DMA . For this i have the following DMA Streams available:
- DMA1 stream 5 - for TIM2_CH1
- DMA1 stream 6 - for TIM2_CH2/CH4
- DMA1 stream 1 - for TIM2_UP/CH3
- DMA1 stream 7 - for TIM2_UP/CH4
The problem i am having is that if I add the DMA1 stream 7 .... stream 6 & stream 1 can no longer be added due to conflicts. In the generated code i see that both events UP & CH4 get linked to this DMA stream so i am guessing that this is why the MX won't let me add the other 2.
Now my question:
- Even though the tool does not allow it since one trigger can be selected for one DMA tream (Channel selection) i think it should be possible to have the following configuration:
- DMA1 stream 5 - for TIM2 CC1
- DMA1 stream 6 - for TIM2 CC2
- DMA1 stream 1 - for TIM2 CC3
- DMA1 stream 7 - for TIM2 CC4
Am i correct ?
Solved! Go to Solution.
2023-07-31 6:26 AM
Yes, you should be able to get the configuration you want, at least in hardware. It's unclear why CubeMX thinks there is a conflict here, probably a bug.
2023-07-31 6:26 AM
Yes, you should be able to get the configuration you want, at least in hardware. It's unclear why CubeMX thinks there is a conflict here, probably a bug.
2023-07-31 6:37 AM
Thank you, figured as much just wanted to be on the safe side and double check.