cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-C071RB Interrupt problem

AndrewFFFF
Associate II

I tried this board but i get some problem about interrupt.

I "writed" only 1 function ( void EXTI0_1_IRQHandler(void) ) the other code has been autmaticaley generate from Cube.

The goal is : for any change of state of PA0, pulse_count++.

The problem is the function "EXTI0_1_IRQHandler(void)" doesn't work it means no interrupt it obtains when the singnal on PA0 chages.. On PA0 there is a square waveform. The uart is died, only because the interrupt doesn't work. I tested the uart and works fine. I cheched hardware problem it seems everything works fine.

Here the code

 

#ifdef __cplusplus
extern "C" {
#endif

#include "main.h"
#include <stdio.h>  
#include <string.h> 
#include "stm32c0xx_hal.h"  
#include "stm32c0xx_hal_gpio.h"
#include "stm32c0xx_hal_tim.h"


#ifdef __cplusplus
}
#endif

volatile uint16_t pulse_count = 0;  






UART_HandleTypeDef huart2;




void SystemClock_Config(void);
static void MX_GPIO_Init(void);

static void MX_USART2_UART_Init(void);


int main(void)
{




  HAL_Init();

  SystemClock_Config();

  MX_GPIO_Init();

  MX_USART2_UART_Init();


  while (1)
  {

  }

}


void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  __HAL_FLASH_SET_LATENCY(FLASH_LATENCY_0);

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV4;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
  RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
  {
    Error_Handler();
  }
}




/**
  * @brief USART2 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_USART2_UART_Init(void)
{

  /* USER CODE BEGIN USART2_Init 0 */

  /* USER CODE END USART2_Init 0 */

  /* USER CODE BEGIN USART2_Init 1 */

  /* USER CODE END USART2_Init 1 */
  huart2.Instance = USART2;
  huart2.Init.BaudRate = 115200;
  huart2.Init.WordLength = UART_WORDLENGTH_8B;
  huart2.Init.StopBits = UART_STOPBITS_1;
  huart2.Init.Parity = UART_PARITY_NONE;
  huart2.Init.Mode = UART_MODE_TX_RX;
  huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart2.Init.OverSampling = UART_OVERSAMPLING_16;
  huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
  huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;
  huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
  if (HAL_UART_Init(&huart2) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetTxFifoThreshold(&huart2, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetRxFifoThreshold(&huart2, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_DisableFifoMode(&huart2) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN USART2_Init 2 */

  /* USER CODE END USART2_Init 2 */

}

/**
  * @brief GPIO Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOA_CLK_ENABLE();

  /*Configure GPIO pin : PA0 */
  GPIO_InitStruct.Pin = GPIO_PIN_0;
  GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

  /* EXTI interrupt init*/
  HAL_NVIC_SetPriority(EXTI0_1_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(EXTI0_1_IRQn);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void EXTI0_1_IRQHandler(void)
{

    if (__HAL_GPIO_EXTI_GET_IT(GPIO_PIN_0) != RESET)
    {
        __HAL_GPIO_EXTI_CLEAR_IT(GPIO_PIN_0);  
        pulse_count ++;
    	char msg[20];
     	sprintf(msg, "Imp: %d\r\n", ((pulse_count*1000/6700))); 
      	HAL_UART_Transmit(&huart2, (uint8_t *)msg, strlen(msg), HAL_MAX_DELAY);

    }
}






void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @PAram  file: pointer to the source file name
  * @PAram  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

2 REPLIES 2
TDK
Guru

> #ifdef __cplusplus

Is this in C++? If so, you will need to use extern "C" as in:

extern "C" void EXTI0_1_IRQHandler() { ...

 

Where is the code execution at when you debug it, toggle the pin, then hit pause?

If you feel a post has answered your question, please click "Accept as Solution".
KnarfB
Principal III

"EXTI0_1_IRQHandler(void)" doesn't work

did you test that by setting a breakpoint?

The uart is died

HAL_UART_Transmit is a blocking function which relies on periodic SysTick interupts for timeout delays. 

Using this in an interrupt context is no good style. At least let the EXTI interrupt have lower priority than the SysTick (STM32CubeMX --> System Core --> NVIC)

Here is a close example: STM32CubeC0/Projects/NUCLEO-C071RB/Examples_LL/EXTI/EXTI_ToggleLedOnIT_Init at main · STMicroelectronics/STM32CubeC0

hth

KnarfB