2019-05-07 6:09 AM
Hi,
I am using cubemx for code generation and i have atollic compiler.
This is first time i am using atollic, previous to that i was using keil and now i have started to use ubuntu. so no keil for ubuntu.
when i generate the code with cubemx, i don't see any makefile there and not project files.
do i need to write makefiles manually?
i googled for the same but didn't get much help.
2019-05-09 6:42 AM
You can generate a project for TrueSTUDIO and then import it and then you're pretty much done and ready to go.
My colleague Mattias did a video that's slightly outdated (new MX design) but it should give you a good idea of how to do it.
You can find it here.