2022-03-29 3:39 AM
Hi I moved a code that was working on STM32CubeIDE v1.8. But after update STM32CubeIDE v1.9 I am facing a new issue that I have never see before in STM32CubeIDE v1.8.0!
I compared what was before and what we have now, see screen...
Maybe to me need only turn on "Auto Negotiation" in main.c and ping will start working but, I don't know how to do it?
Could someone tell me why code do not initialize MX_LWIP_INIT (); ?
 
Bellow my simple code main.c
/* USER CODE BEGIN PV */
extern struct netif gnetif;
/* USER CODE END PV */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
ethernetif_input(&gnetif);
sys_check_timeouts();
}
/* USER CODE END 3 */
}
Solved! Go to Solution.
2022-03-29 12:11 PM
Should look at the LWIP_RAM_HEAP_POINTER definition
0x30044000 doesn't strike me as a valid RAM region in the STM32F4 devices.
Make sure it's building for the right target
2022-03-29 9:20 AM
No, I was wrong when I thought that to me need just activate "Auto Negotiation" it is already activated in stm32f4xx_hal_conf.h
Any ideas?
2022-03-29 9:26 AM
>>Any ideas?
Hard Faults, diagnose what's actually causing it, and work the issue from there.
Look at the faulting instructions/code, see what it is doing.
Faulting in random locations, perhaps look at interrupts, handlers, call-backs.
Faulting in the same place, likely errant pointers, memory usages or corruption.
Check stack
2022-03-29 9:40 AM
How to find out what's actually causing it?
I'm debugging it and it write to my nothing.
After the underlined line on attached screen code immediately flies into "void HardFault_Handler(void)"
2022-03-29 12:11 PM
Should look at the LWIP_RAM_HEAP_POINTER definition
0x30044000 doesn't strike me as a valid RAM region in the STM32F4 devices.
Make sure it's building for the right target
2022-03-29 12:35 PM
THANK YOU!!!!!!!!!!!!!!!!!
Everything start working after commented "LWIP_RAM_HEAP_POINTER" for stm32f407vg!
Is it possible to disable "LWIP_RAM_HEAP_POINTER" in GUI?