2017-05-10 1:44 AM
Hi
the TSC library built in cubeMX repositories is not consitent.
Where do I find the evry latest release?
in STM32Cube_FW_L4_V1.7.0/ this version is used: V2.2.0 / 01-February-2016
in STM32Cube_FW_L0_V1.9.0/ this version is used: V2.0.0 / 22-April-2014
see release notes under
STM32Cube/Repository/********Middlewares/ST/STM32_TouchSensing_Library/Release_Notes.html
#tsc #stm32-cubemxSolved! Go to Solution.
2017-05-10 9:18 AM
Yes, currently this is the one embedded in other packages.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-05-10 4:29 AM
Hi
dieter.dieter
,I agree with you that we have to align versions of libraries embedded in our STM32Cube packages.
Your remark is valid and is reported internally asking to use the same version ofSTM32_TouchSensing_Library in CubeL0 as other packages (L4/F3/F0).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-05-10 9:15 AM
Thanks
st.mcu
and what is the latest version? this one?::::: V2.2.0 / 01-February-2016
2017-05-10 9:18 AM
Yes, currently this is the one embedded in other packages.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-12-14 1:39 AM
Hello,
The last version of Touch library (V2.2.0 / 01-February-2016) is embedded in STM32CubeL0 V1.11.0.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.