cancel
Showing results for 
Search instead for 
Did you mean: 

Issue in FW F7 HAL package 1.17.x

Petr3
Associate III

Hi,

i have STM32F767BIT6 MCU and microcontroller crashes into Hard Fault during initialisation of LWIP MX_LWIP_Init(); Problem is that in FreeRTOS is calling memcpy in queue.c in function prvCopyDataFromQueue with huge ammount of length.

( void ) memcpy( ( void * ) pvBuffer, ( void * ) pxQueue->u.xQueue.pcReadFrom, ( size_t ) pxQueue->uxItemSize );

Source(pxQueue->u.xQueue.pcReadFrom) and destination(pvBuffer) address is correct placed inside internal SRAM area but length(pxQueue->uxItemSize) is so huge, that end address is placed out of accessible area. So it goes into HardFault_Handler.

 

When i created the same project in older STM32cubeIDE 1.6 (FW F7 package 1.16.x) it works fine but when i create project with newer STM32cubeIDE (1.10 or 1.12 or 1.14) with FW F7 package 1.17.x it crashes into HardFault_Handler.

 

Best regards,

Petr

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Petr3
Associate III

I agree, the stack extension helps and it works with it.

Thank you for help.

CMYL
ST Employee

Good news, You are welcome :)