2021-01-08 3:31 AM
2021-01-08 3:35 AM
Hi @JCool.1
You need to add the STM32CubeMX Topic when you want to report an issue with CubeMX.
Now you're in the right direction.
Khouloud
2021-01-08 3:40 AM
2021-01-11 5:52 AM
2021-01-11 6:57 AM
2021-01-21 2:08 AM
2021-01-21 3:29 AM
2021-01-21 5:49 AM
Hi @JCool.1
I did not receive any email about this subject, can you please re-check ?
Thanks, Khouloud
2021-01-21 6:39 AM
2021-01-26 5:39 AM
Hello @JCool.1 ,
I think I understood the problem which prevents the appearance of your attached files, indeed, it is necessary to answer manually to this conversation, ie, you need to click on "view" when you will receive a notification of my comment or on this link and not on "reply to this email", then add your files as mentioned on the image below.
Thanks, Khouloud