cancel
Showing results for 
Search instead for 
Did you mean: 

Is the STM32H747 code directly portable to the STM32H757?

jmorganj
Associate III

I'm using the STM32H757i Eval board. In STMCube repository for H7 v1.10.0, there is not a project folder for the STM32H757i eval board. I'd like to use the BSP LED/Touch drivers from the STM32H747i-EVAL project found in the cubeMX repository and potentially any others in the future. From what I could understand from UM2525, the eval boards are the same except for the actual micro-controllers.

Can I start a project with the STM32H757 project and link to the folder with the STM32H747 eval files?

Or, can I start a project in CubeMX for the STM32H747 and upload it to the STM32H757 allowing me to use any driver code written for the STM32H747i eval board.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Uwe Bonnes
Chief

The H757 is code compatible to the H747, so yes , you can run H747 code on the H757.

View solution in original post

1 REPLY 1
Uwe Bonnes
Chief

The H757 is code compatible to the H747, so yes , you can run H747 code on the H757.