2024-09-29 6:34 PM
I am using STM32CubeMX and need to set
nBoot0, nBOOT0_SEL, and BOOT_LOCK. (Stm32G031 series is being used and Pattern 11 is being used)
I have difficulty connecting with the STM32Cubeprogrammer program,
so I would like to process it with the CubeMX program if possible,
but I would like to inquire about how to modify the register.
Please let me know!! please.
Solved! Go to Solution.
2024-09-29 7:13 PM
STM32CubeMX cannot modify option bytes as it doesn't connect to the chip at all.
STM32CubeProgrammer is the easiest way to program them. If you're having trouble connecting, I would suggest figuring out why and solving that issue rather than hoping another program will work better.
2024-09-29 7:13 PM
STM32CubeMX cannot modify option bytes as it doesn't connect to the chip at all.
STM32CubeProgrammer is the easiest way to program them. If you're having trouble connecting, I would suggest figuring out why and solving that issue rather than hoping another program will work better.
2024-09-29 7:17 PM
The STM32G031 DSP seems to have stopped working after performing a firmware update. Is this because the boot settings are not set?
2024-09-29 7:20 PM
No, unless those settings were changed in the firmware update. Which they probably weren't.
2024-09-29 7:23 PM
I performed a firmware update without boot settings, and it worked once. But when I tried it the second time, it didn't connect at all. Will it be restored if I set up a boot connection?
2024-09-29 7:39 PM
You may need to explain your situation more.
What device are you working with? What "firmware update" did you do? And how was that firmware update done?
2024-09-29 7:43 PM
I used a product called 'Easy Dsp' and installed firmware designed by STM32CubeMX.
However, after performing the update once, the DSP seems to have stopped.
I think it's related to boot settings, and I'm trying to modify boot pins using STM32Programmer.