cancel
Showing results for 
Search instead for 
Did you mean: 

In CubeMX, why are some chip pins shown in dashed boxes?

Leslie_Yuan
Associate

Leslie_Yuan_0-1726798401306.png

In CubeMX, why are some chip pins shown in dashed boxes? 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

This is a UFQFN48 chip, which doesn't have leads. It shows in the dashed boxes because the pads are on the bottom of the chip and it's trying to visually replicate the layout.

TDK_0-1726803965724.png

 

On LQFP they're shown on the outside of the chip. On BGAs they're shown as circles on the chip where the balls are underneath.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
Karl Yamashita
Lead III

What do you mean by "dashed boxes"?

Or do you mean by dashes in the names? If the names, then it's just long names that don't fit. If you hover over the pins then you'll see the full name

Tips and Tricks with TimerCallback https://www.youtube.com/@eebykarl
If you find my solution useful, please click the Accept as Solution so others see the solution.
TDK
Guru

This is a UFQFN48 chip, which doesn't have leads. It shows in the dashed boxes because the pads are on the bottom of the chip and it's trying to visually replicate the layout.

TDK_0-1726803965724.png

 

On LQFP they're shown on the outside of the chip. On BGAs they're shown as circles on the chip where the balls are underneath.

If you feel a post has answered your question, please click "Accept as Solution".

That makes sense! Thank you for your reply!