cancel
Showing results for 
Search instead for 
Did you mean: 

setting sequencer option to "fully configurable" hides channels IN17...IN22. Why?

curiocity
Associate III

 

In CUBE MX I have selected the microcontroller STM32C071CBT6 When I set the sequencer option to "sequencer set to fully configurable" then the channels IN17 IN18 IN19 IN20 IN21 IN22 are hidden why?  is there any limitation for that channels or anything else?

1 ACCEPTED SOLUTION

Accepted Solutions
KnarfB
Super User

 then the channels IN17 IN18 IN19 IN20 IN21 IN22 are hidden

correct. See reference manual  RM0490 Rev 5, 16.4.8 Channel selection (CHSEL, SCANDIR, CHSELRMOD).

Why? The ADC_CHSELR register uses 4-bit per channel in that mode.

hth

KnarfB

 

View solution in original post

2 REPLIES 2
KnarfB
Super User

 then the channels IN17 IN18 IN19 IN20 IN21 IN22 are hidden

correct. See reference manual  RM0490 Rev 5, 16.4.8 Channel selection (CHSEL, SCANDIR, CHSELRMOD).

Why? The ADC_CHSELR register uses 4-bit per channel in that mode.

hth

KnarfB

 

Thanks that helps me