cancel
Showing results for 
Search instead for 
Did you mean: 

I can not trust the MX plugin to generate the right code. I cannot get the serial port to work at all with the generated code. It used to work no problem.

KiptonM
Lead

First the GUI is all screwed up.

When I look at USART2 It gives me the choices for

GPIO output level,

GPIO mode,

GPIO Pull-up/Pull-down

Maximum output speed

User Label,

it is missing Fast Mode.

0693W00000NsptCQAR.pngI click down to USART1_TX and the list is different. It has

GPIO mode,

GPIO Pull-up/Pull-down

Maximum output speed,

Fast Mode

User Label

This one is missing GPIO Output Level.

And it says it is "Modified" I told it to revert to the default and it is still "Modified"

0693W00000NspvDQAR.png 

This is a known problem, but it does not help me that it is known.

Here is the code generated.

/**
  * @brief USART1 Initialization Function
  * @param None
  * @retval None
  */
static void MX_USART1_UART_Init(void)
{
 
  /* USER CODE BEGIN USART1_Init 0 */
 
  /* USER CODE END USART1_Init 0 */
 
  /* USER CODE BEGIN USART1_Init 1 */
 
  /* USER CODE END USART1_Init 1 */
  huart1.Instance = USART1;
  huart1.Init.BaudRate = 115200;
  huart1.Init.WordLength = UART_WORDLENGTH_8B;
  huart1.Init.StopBits = UART_STOPBITS_1;
  huart1.Init.Parity = UART_PARITY_NONE;
  huart1.Init.Mode = UART_MODE_TX_RX;
  huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart1.Init.OverSampling = UART_OVERSAMPLING_16;
  huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
  huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
  huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
  if (HAL_UART_Init(&huart1) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
  {
    Error_Handler();
  }
  if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN USART1_Init 2 */
 
  /* USER CODE END USART1_Init 2 */
 
}

It looks good. I do not see an error in it. Can anyone else?

In my main program it has

int main(void)
{
  /* USER CODE BEGIN 1 */
 
  /* USER CODE END 1 */
 
  /* MCU Configuration--------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
  /* USER CODE BEGIN SysInit */
 
  /* USER CODE END SysInit */
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_DMA_Init();
  MX_ADC1_Init();
  MX_I2C1_Init();
  MX_TIM2_Init();
  MX_TIM3_Init();
  MX_TIM14_Init();
  MX_USART2_UART_Init();
  MX_USART1_UART_Init();
 
  /* Initialize interrupts */
  MX_NVIC_Init();
  /* USER CODE BEGIN 2 */
 
  uint8_t data[] = "Hello World ***********\r\n";
 
  HAL_UART_Transmit(&huart1, data, sizeof(data), 100);
 
  HAL_Delay(250);
  __NOP();

I put a break point at the __NOP();

The logic analyzer says the UART1 TX pin did not move at all.

The serial port used to work. I like to use it for debugging. I print messages out to see what is going on when it is running. So it is the first thing I get to work when I bring up a new board. The pinout of the STM32G031K6T and STM32G051K8T are exactly the same and both have USART1 and USART2 to the same pins.

Because the MX does not transition from one chip to another (another bug that will be fixed in another version) I started another project. And am trying to bring it up peripheral by peripheral, and USART1 is the first one. The clocks are setup the same. 64 MHz in both cases.

,

I do not trust the latest MX add-in or anything about it, but I do not see what could cause it not to work even in polling mode.

Thanks,

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Sara BEN HADJ YAHYA
ST Employee

Hello @KiptonM​ ,

Yes the issue is also fixed in CubeIDE.

Before performing project migration to the latest version v1.10.0 please check this thread first.

Sara.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
KiptonM
Lead

Too late for me. I just updated like the STM32CubeIDE program instructed.