2020-07-30 10:15 PM
2020-08-03 5:40 AM
Hello BButl.1,
The use of Java Run Time Environment 1.8_45 64-bit is strongly advised to prevent the unavailability of some features such as code generation for the STM32CubeIDE toolchain. Limited validation is done with Java™ 11. Java™ 7, Java™ 9, Java™ 10, and Java™ 13 are not supported.
More information on installation requirements and procedure is in the STM32CubeMX for STM32 configuration and initialization C code generation user manual (UM1718).
BR,
Khouloud.