cancel
Showing results for 
Search instead for 
Did you mean: 

how can connected STM32F407 with PC ? how can used UART port correctly ?

alouni bargougui
Associate II

please i need some help 

i used UART to communicate stm32f407vg tx dicovery

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

USART1 PA9/PA10 is not viable due to a capacitor on one of the lines.

Use USART6 PC6/PC7

The USART signals at CMOS levels, this is not compatible with RS232, you will need a MAX3232 type device to shift levels if using RS232 connectivity.

You may use a USB-to-CMOS Serial adapter/dongle, FTDI or SiLabs type chips.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

thank you Clive Two.Zero

i used usb ttc adaptator

i need to use TIM or not ?

The USART peripheral functions independently of the TIM and other peripherals. Your library may established other requirements for timeouts etc, ie HAL with SysTick

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

thanks

i need USART to read some value from inerface labview, are you have any information how excecute this communication ?

thanks a lot