2024-04-19 4:11 AM - edited 2024-04-19 4:30 AM
So I've moved away from eclipse and the CubeMX IDE.
I am using sublime as my editor and I am enjoying a great deal of success and I would recommend to anyone using cubemx to migrate to a non java based IDE/editor - I compile the makefiles generated from CubeMX IDE and upload using STM32_Programmer_CLI directly from sublime.
Therefore, as I want to forgo eclipse (except for debugging, the build analyser, and a few nice tools within)
My questions are:
How does CUBEMX generate the makefiles. (I assume it requires the .mxproject and or .cproject files but I would be happy to edit those myself if required)
Can I run a command/script to achieve the same end?
If not, it appears that CUBEMX only updates the makefiles when you perform a build. Can I at least stop compilation when running Debug/Build?
Thanks for any suggestions
+ sorry for initially posting this in the wrong part of the forum
2024-04-19 4:22 AM
You are confusing CubeMX and CubeIDE:
Actually, it should be enough if you only install CubeMX and use its generated source code and e.g. the makefile - unless you don't want to use a Java-based tool at all.
Hope that helps?
Regards
/Peter
2024-04-19 4:29 AM - edited 2024-04-19 4:34 AM
Thanks Peter. Sorry about the incorrect name of the IDE.:(
Doesn't CubeMx (not CubeIDE in this instance) only generate your first draught (from an .ioc file)?
Then any changes are handled in STM32IDE, no?
What if I am continuously change the codebase? (I don't use .ioc anymore)
Thanks for the support
2024-04-19 4:42 AM
@Claydonkey wrote:Then any changes are handled in STM32IDE, no?
Depends what you mean by "changes".
If you go back to CubeMX (or the equivalent within CubeIDE), make changes there, and re-generate then that will update the existing project.
Other changes to the project, eg, adding/removing/reorganising source files) are handled by CubeIDE.
2024-04-19 4:47 AM - edited 2024-04-19 4:52 AM
Thanks for the reply Andrew. I don't think CubeMX is the solution as I won't be generating from ioc files. As far as I can see in CubeMX, it loads projects as ioc files. So by that reckoning it generates boilerplate to get you up and running.
It seems to me that I will look at the makefiles and probably will write a cmake based on that. https://github.com/ObKo/stm32-cmake looks promising.
2024-04-19 6:21 AM
Lo and behold. CubeMX can now generate CMake. But it's still "beta quality".