cancel
Showing results for 
Search instead for 
Did you mean: 

Generate adjustable single short pulse (using timer ?)

Valentin Gros
Associate III

Hello,

I want to generate a single short pulse (adjustable between 100 ns to 1ms). What is the best way ?

I think we should use timers, but which mode ? (which CubeMX configuration ?)

Moreover I tried to configure one-pulse mode but I can't find documentation or tutorial. Either my settings (trigger mode...) are wrong, either I don't have the proper HAL command to initialise or start the pulse. Which HAL functions are needed ?

Thank you,

Valentin

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0