2017-09-24 12:48 PM
I have generated a project using the GPDSC format for STM32L151CC MCU and there are several 'LL' driver files missing from that output file. For example 'stm32l1xx_ll_gpio.c.'
In the configuration for the peripherals all are selected to 'LL' driver.
CubeMX is v4.22.0
Please advise how I can resolve this,
Sid
#gpdsc #cubemx2017-09-24 4:25 PM
Aren't the HAL and LL files under the L1 driver tree?
..\Drivers\STM32L1xx_HAL_Driver
Can you copy the files from there, or add into the project?
2017-09-24 6:31 PM
Well yes they are, however I am processing the GPDSC file into our build system and that file doesn’t contain all the required files, so the build system doesn’t know which to include
Sid
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.