2023-03-21 03:31 AM
When I try to migrate project (.ioc) from STM32CubeMX V6.5.0 to STM32CubeMX V6.8.0 (STM32Cube FW_F3 V1.11.4 used) the following hint pops up:
After selection of 'Migrate' or 'Continue' the following error pops up:
My question:
Is there a way to migrate STM32CubeMX-Project-File without using STM32CubeIDE?
Rowley CrossWorks for ARM is used for code development.
Solved! Go to Solution.
2023-03-21 04:39 AM
The question can be deleted. Problem was solved.
The warning was misinterpreted.
2023-03-21 04:39 AM
The question can be deleted. Problem was solved.
The warning was misinterpreted.
2023-03-21 05:25 AM
Well, it's always a good idea to leave the question and insert the answer, even if it was your own mistake - the next user with the same problem will surely be pleased. Thank you very much for your support!
When your question is answered, please mark this topic as answered by choosing Select as Best for the preferred answer. This will help other users find that answer faster.
Regards
/Peter