cancel
Showing results for 
Search instead for 
Did you mean: 

Does CubeMX skip GPDMA channel init when switching from Software to a peripheral request?

Tzahi14
Associate

Hi,

I'm using STM32CubeIDE 1.18.1v, which includes STM32CubeMX 6.14.1v, and I'm seeing unexpected behavior when working with GPDMA1 on an STM32H5 device.

When I configure a DMA channel with Request set to "Software", CubeMX generates full initialization code.

However, as soon as I change the Request to any other peripheral trigger, for example TIM2_CH1, all of the DMA configuration disappears from the generated code. Only the RCC clock enable and interrupt configuration remain.

 

Example 1 — Request = Software:

static void MX_GPDMA1_Init(void) { /* USER CODE BEGIN GPDMA1_Init 0 */ /* USER CODE END GPDMA1_Init 0 */ DMA_NodeConfTypeDef NodeConfig = {0}; /* Peripheral clock enable */ __HAL_RCC_GPDMA1_CLK_ENABLE(); /* GPDMA1 interrupt Init */ HAL_NVIC_SetPriority(GPDMA1_Channel0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(GPDMA1_Channel0_IRQn); /* USER CODE BEGIN GPDMA1_Init 1 */ /* USER CODE END GPDMA1_Init 1 */ NodeConfig.NodeType = DMA_GPDMA_LINEAR_NODE; NodeConfig.Init.Request = DMA_REQUEST_SW; NodeConfig.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST; NodeConfig.Init.Direction = DMA_MEMORY_TO_MEMORY; NodeConfig.Init.SrcInc = DMA_SINC_FIXED; NodeConfig.Init.DestInc = DMA_DINC_FIXED; NodeConfig.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_BYTE; NodeConfig.Init.DestDataWidth = DMA_DEST_DATAWIDTH_BYTE; NodeConfig.Init.SrcBurstLength = 1; NodeConfig.Init.DestBurstLength = 1; NodeConfig.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0; NodeConfig.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER; NodeConfig.Init.Mode = DMA_NORMAL; NodeConfig.TriggerConfig.TriggerPolarity = DMA_TRIG_POLARITY_MASKED; NodeConfig.DataHandlingConfig.DataExchange = DMA_EXCHANGE_NONE; NodeConfig.DataHandlingConfig.DataAlignment = DMA_DATA_RIGHTALIGN_ZEROPADDED; NodeConfig.SrcAddress = 0; NodeConfig.DstAddress = 0; NodeConfig.DataSize = 0; if (HAL_DMAEx_List_BuildNode(&NodeConfig, &Node_GPDMA1_Channel0) != HAL_OK) { Error_Handler(); } if (HAL_DMAEx_List_InsertNode(&List_GPDMA1_Channel0, NULL, &Node_GPDMA1_Channel0) != HAL_OK) { Error_Handler(); } if (HAL_DMAEx_List_SetCircularMode(&List_GPDMA1_Channel0) != HAL_OK) { Error_Handler(); } handle_GPDMA1_Channel0.Instance = GPDMA1_Channel0; handle_GPDMA1_Channel0.InitLinkedList.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT; handle_GPDMA1_Channel0.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION; handle_GPDMA1_Channel0.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT1; handle_GPDMA1_Channel0.InitLinkedList.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER; handle_GPDMA1_Channel0.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR; if (HAL_DMAEx_List_Init(&handle_GPDMA1_Channel0) != HAL_OK) { Error_Handler(); } if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel0, &List_GPDMA1_Channel0) != HAL_OK) { Error_Handler(); } if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel0, DMA_CHANNEL_NPRIV) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN GPDMA1_Init 2 */ /* USER CODE END GPDMA1_Init 2 */ }
View more

 

Example 2 — Request = TIM2_CH1:

static void MX_GPDMA1_Init(void) { /* USER CODE BEGIN GPDMA1_Init 0 */ /* USER CODE END GPDMA1_Init 0 */ /* Peripheral clock enable */ __HAL_RCC_GPDMA1_CLK_ENABLE(); /* GPDMA1 interrupt Init */ HAL_NVIC_SetPriority(GPDMA1_Channel0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(GPDMA1_Channel0_IRQn); /* USER CODE BEGIN GPDMA1_Init 1 */ /* USER CODE END GPDMA1_Init 1 */ /* USER CODE BEGIN GPDMA1_Init 2 */ /* USER CODE END GPDMA1_Init 2 */ }

 

Is this expected behavior when using a peripheral request instead of Software?
Or should CubeMX generate the same kind of init code regardless of the request type?

Thanks in advance!

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @Tzahi14 ,

 

By changing the Request to [any other peripheral trigger], you find the DMA Configuration on the stm32h5xx_hal_msp.c file.

 

MahmoudBenRomdhane_0-1745237752201.png

 

Thanks.

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Mahmoud Ben Romdhane
ST Employee

Hello @Tzahi14 ,

 

First let me thank you for your post and welcome to the ST Community.

I am currently investigating your request, and I will get back to you ASAP.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @Tzahi14 ,

 

By changing the Request to [any other peripheral trigger], you find the DMA Configuration on the stm32h5xx_hal_msp.c file.

 

MahmoudBenRomdhane_0-1745237752201.png

 

Thanks.

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.