2025-01-01 10:52 AM
Hi,
I am trying to find a solution to support different build configurations for the same MCU but different revision of PCB builds. PCB revisions could happen because of reassignment of pins and peripherals. I am using standalone version of CubeMX to generate code. So, I will end up with two different .ioc files for each revision and when I generate code, 2 separate project files are generated.
Is there a way to have a single project, but 2 different build configurations for each ioc file? Looks like CubeMX doesn't support this, but are there any tricks as a workaround ?
Solved! Go to Solution.
2025-01-01 11:29 AM
A single project should be based on a single .ioc file. It is not possible to have a project based on a new .ioc file each Time.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-01 11:15 AM
Hello @kraman2024
Could you please give more details about what you are looking for (an example of a use case Will really do the job).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-01 11:18 AM
I want to maintain 2 different ioc files for 2 different hardware revisions of a custom board. I want a single project either EWARM or Cube IDE project to support these 2 revisions of the board as separate build configurations. Is this possible?
2025-01-01 11:29 AM
A single project should be based on a single .ioc file. It is not possible to have a project based on a new .ioc file each Time.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.