cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX install on Mac Sierra

Sebastian G.
Associate II
Posted on December 06, 2016 at 09:52

I am trying to install CubeMX 4.18.0 on my Mac (Sierra), opening the installer appears to do nothing, if launched via spotlight i get a warning stating unable to open the programm.

#cubemx #macos #sierra
13 REPLIES 13
Nesrine M_O
Lead II
Posted on December 06, 2016 at 10:45

Hi

nathancdc

,

Please refer to the

/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fresource%2Fen%2Fuser_manual%2Fdm001047pdf

user manual and follow the steps/requirements for installing and running CUBEMX under MacOS:

  • Make sure that tyou have administrators rights.

  • Make sure that you haveinstalled Java Development Kit 1.7.0_45 or later.

    If the issue persist again please contact us.

-Nesrine M-

Posted on December 06, 2016 at 11:47

I got admin rights and 'javac 1.8.0_102' -> already had cubemx installed a while ago, so it was running on this exact computer. Dont know what changed!?

Posted on December 06, 2016 at 11:54

Hi

nathancdc

,

I'll report this issue to our MX team for checking. Sorry for the inconvenience it may bring.

-Nesrine M-

Posted on December 06, 2016 at 15:44

I installed the eclipse add-on, it runs and does everything i need!

Fleck
Associate II
Posted on December 23, 2016 at 20:09

Double-clicking the installer didn't work for me either.

Workaround: open a terminal, cd to the directory where the files have been unpacked and start the installer with the command:

java -jar SetupSTM32CubeMX-4.0.exe
�?

This worked for me.

Posted on January 09, 2017 at 07:12

I had a same problem and this worked for me Thanks!

Kirill Makukhin
Associate
Posted on May 16, 2017 at 05:50

Installing with sudo works:

sudo open 'path_to_/SetupSTM32CubeMX-4.21.0.app'

However, it screws automatic update
Heath Raftery
Associate II
Posted on July 13, 2017 at 09:29

This was killing me too - silent failure. Eventually discovered I could cd to SetupSTM32CubeMX-4.22.0.app/Contents/MacOs and run the executable from the command line:

$ cd ~/Downloads/en/SetupSTM32CubeMX-4.22.0.app/Contents/MacOs

$ ./SetupSTM32CubeMX-4_22_0_macos

Please install Java JDK 1.7.0_45 or a more recent version

Hallelujah! Just needed to install the latest JDK (not the JRE as directed elsewhere!) and away we go.

Thierry Coton
Associate
Posted on October 19, 2017 at 22:38

Actually, the setup for Mac OS has been copied from a Linux installation and can only stall as the setup is trying to write into /usr/share/applications which does not exists on Mac OS but does not pop any error up...

LOL, seriously, guys, do you really have a Mac?

:)

 

I had to open the package and launch the setup in a terminal to discover this.

It has been a year this issue exists and still not fixed.

/Users/***********/Downloads/en.stm32cubemx/SetupSTM32CubeMX4.22.1.app/Contents/MacOs/SetupSTM32CubeMX-4_22_1_macos ; exit;

iMac-**-*****:~ **********$ /Users/***********/Downloads/en.stm32cubemx/SetupSTM32CubeMX4.22.1.app/Contents/MacOs/SetupSTM32CubeMX-4_22_1_macos ; exit;

19 oct. 2017 16:19:14 INFOS: Logging initialized at level 'INFO'

19 oct. 2017 16:19:14 INFOS: Commandline arguments:

19 oct. 2017 16:19:15 INFOS: Detected platform: mac_osx,version=10.12.6,arch=x86,symbolicName=null,javaVersion=9.0.1

19 oct. 2017 16:19:18 WARNING: Cannot write to '/usr/share/applications'