2023-11-12 04:13 AM
2023-11-12 04:46 AM
Hello @Rxt_Master and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I've succeeded to generate the code based on the .ioc file that you added to this post. I suggest you use the last versions of CubeMX and CubeIDE. Also, it will better if you restart your PC.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-12 05:13 AM
Thank you for your answer, but my cubeMX is already the latest version, and I have also tried restarting, but it does not work
2023-11-12 05:17 AM
If I don't use freertos, I can generate the code normally
2023-11-12 05:41 AM
I tried it on my classmate’s computer. He also installed the latest version and encountered the same problem.
2023-11-12 05:48 AM
and I am using windows system
2023-11-12 10:09 AM
@Rxt_Master Is your school IT available to help? Do they install any "security" software on your computers, besides of the Windows "defender"? If so, try to disable it temporarily?
2023-11-12 12:46 PM
I had a similar problem today.
- Be patient, after some time it came through.
- Be sure you are logged on.
- Be aware of message boxes asking for confirmation related to licenses.
2023-11-13 02:54 AM
I've tried turning off the firewall and anti-virus software, but it still doesn't work