2024-03-03 7:24 AM
CMSIS need to be updated to the new version.
The version 6 changes some register name in header file.(Drivers\CMSIS\Core\Include\core_cm4.h etc.)
Tested on MCU package F3 v1.11.4 and G0 v1.6.2. Guessing all MCU package using CMSIS v5.0.3.
Solved! Go to Solution.
2024-03-05 7:19 AM - edited 2024-03-05 7:20 AM
Hello @Zack
I've escalated your request internally to the concerned team for analysis and further investigation (through Internal ticket number: 175309)
(PS: Internal ticket number 175309 is only for reference, not available outside of ST).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-03 9:52 AM
Hello @Zack
As you can see in this post. This request has been escalated internally to CubeMX team for analysis and further investigation.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-03 11:39 PM
Hi @STTwo-32
Not quite the same as in the post.
The default CMSIS header file used in STM32Cube Firmware Package needs to be upgraded to version V6.
As an example:
STM32Cube\Repository\STM32Cube_FW_F3_V1.11.4\Drivers\CMSIS\Core\Include\core_cm4.h
SCB->SHP changed to SCB->SHPR in cmsis v6(not Keil v6) and in some cases (e.g. CubeMX generating a Keil project, adding rtos-rtx in Keil) will result in compilation errors.
2024-03-05 7:19 AM - edited 2024-03-05 7:20 AM
Hello @Zack
I've escalated your request internally to the concerned team for analysis and further investigation (through Internal ticket number: 175309)
(PS: Internal ticket number 175309 is only for reference, not available outside of ST).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.