2024-10-21 4:15 PM - edited 2024-10-21 4:17 PM
Trying to export LQFP144 pinout to Altium CAD models with cubeMX.
But CubeMX is trying add pin #204 #202 #158, etc, on symbol for an L471 micro that doesn't even come in packages bigger than 144 pins. Altium chokes on this symbol, I imagine that's because the foot print only has 144pins.
See screenshot below. Will attach .ioc file if possible.
Solved! Go to Solution.
2025-03-06 12:51 AM
Hello @DixonDon,
This issue is fixed, please check new STM32CubeMX-6.14.0 published on st.com
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-22 2:00 AM - edited 2024-10-22 2:09 AM
Hello @DixonDon,
Thank you for spotting this!
This behavior will be investigated by the STM32cubeMX team (Internal ticket number: 194578), meanwhile, as a temporary workaround, you can manually edit the symbol in Altium Designer to remove the incorrect pins
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-06 12:51 AM
Hello @DixonDon,
This issue is fixed, please check new STM32CubeMX-6.14.0 published on st.com
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.