cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX CAD models mixing LQFP144 and 208pinouts

DixonDon
Associate II

Trying to export LQFP144 pinout to Altium CAD models with cubeMX.  

But CubeMX is trying add pin #204 #202 #158, etc, on symbol for an L471 micro that doesn't even come in packages  bigger than 144 pins.  Altium chokes on this symbol, I imagine that's because the foot print only has 144pins.

See screenshot below.  Will attach .ioc file if possible.

 

Screenshot 2024-10-21 180625.png

1 ACCEPTED SOLUTION

Accepted Solutions
Sarra.S
ST Employee

Hello @DixonDon

This issue is fixed, please check new STM32CubeMX-6.14.0 published on st.com

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Sarra.S
ST Employee

Hello @DixonDon

Thank you for spotting this! 

This behavior will be investigated by the STM32cubeMX team (Internal ticket number: 194578), meanwhile, as a temporary workaround, you can manually edit the symbol in Altium Designer to remove the incorrect pins 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Sarra.S
ST Employee

Hello @DixonDon

This issue is fixed, please check new STM32CubeMX-6.14.0 published on st.com

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.