‎2018-12-21 11:36 AM
Hello,
All the time I re-generate the code in CubeMX5 it deletes all my code in the main.c
I have Mac OS High Sierra and use SW4STM32, working with MCU STM32F103C8.
I tried all the options in the Code Manager / Code generation tab and nothing
Edit1:
I notice some code is left outside the main loop, otherwise all code inside the main() disappear.
I also tried the old version of CubeMX 4.27 and the same problem arrises. I wonder if it has something to do with SW4STM32.
Edit2:
I uninstalled everything and re-installed again, it seems to be working now. I am not sure what was the problem. I will keep you updated if problem arises again.