2019-02-25 4:17 PM
Hi. I am using CubeMX code generation for the STM32F767VITx. I recently updated to CubeMX 5.1.0. Since updating, every time I choose to generate code, I get the following warning:
" - These IPs still have some not configured or wrong parameter values: [GFXSIMULATOR]" However, GFXSimulator is not used as a part of this project and has not had any of its parameters changed.
As far as I can tell there appears to be no way to actually disable the GFXSimulator itself, and no amount of clicking 'Reset Configuration' will make the warning disappear. The only method I have found to actually make the warning disappear is to set my clock to 200MHz, but I cannot use that clock speed for the project and that "fix" only seems to work half of the time.
This issue does occur on a blank new CubeMX project for the STM32F767VITx.
In addition, when this occurs a pair of files named 'gfxsimulator.c' and 'gfxsimulator.h' are generated, both of which contain a bunch of empty method declarations.
Any help would be appreciated.
2019-03-01 12:04 PM
The same issue after migration from a 5.0.0 project to 5.1.0 for a NUCLEO F429ZI. No use of GFXSIMULATOR configured in previous version.
2019-03-01 4:37 PM
CubeMX5.1.0生�?SW4STM32代�?第一次正确,�?新生�?之�?�,STM32F767IGTx_FLASH.ld�?��?空文件,file size = 0。怎么办?
2019-03-01 9:02 PM
As all tools, bugs lurks around. Most important is to check the generated code and see if it looks ok for debugging.
2019-03-13 6:44 AM
Same for me. Migrated from previous version and GFXSIMULATOR is selected. Can't find any way to disable this function.
2019-04-27 10:54 AM
Same for me on a Nucleo-f746zg, but only after I enable the Interrupt of any function (tested with SPI and Timers).