cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX v4.27.0 Do not generate main() doesn't set in GUI, when re-opening project file

kurta999
Senior

I opened a project, upgraded to new CubeMX. Checked this option, regenerated the project. After re-opening the CubeMX file, this option is still set, because generation work correctly (no main() generated), but GUI isn't show it as set. The "set" sign (idk what is proper name for this :)) is missing.

After opening settings tab, clicking on OK will result in re-generating main().

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
Khouloud GARSI
ST Employee

Hi @kurta999​ ,

This is reported internally for further check.

Sorry for any inconvenience this may have caused.

Khouloud.

Houda GHABRI
ST Employee

Hello @kurta999​ ,

Sorry for the late response.

I'm not able to reproduce the issue with STM32CubeMX v4.27.0 (migrated from 4.26.1).

Could you please send me the ioc.

Regards,

Houda

kurta999
Senior

It's still bugged in 5.0.1, sadly.

kurta999
Senior

Is this bug planned to be fixed in near futire? Tested with 5.1.0, sadly still nothing changed.

kurta999
Senior
 
Khouloud ZEMMELI
ST Employee

​Hello @kurta999​ 

Sorry for the delay in answering,

I have reported this issue and it will be fixed in the next CubeMX release.

Sorry again and thank you for the feedback.

Best Regards,

Khouloud.

kurta999
Senior

Thank you!

kurta999
Senior

Is this bug planned to be fixed in near future? Tested with CubeMX 5.2.0, same behaviour as before. Nothing changed.