cancel
Showing results for 
Search instead for 
Did you mean: 

[BUG] STM32 lwIP ethernetif.c incorrect error evaluation in low_level_output()

Jak
Associate

Jak_0-1713354570879.png

When HAL_ETH_Transmit_IT() returns an error the errval variable is not changed from ERR_OK to reflect that in the else section.

1 REPLY 1
Semer CHERNI
ST Employee

Hello @Jak 

First let me thank you for posting.

Could you provide more details about the project configuration:

  • The CubeMX version used
  • The used MCU
  • If possible the ioc file to be able to reproduce the issue.

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.