cancel
Showing results for 
Search instead for 
Did you mean: 

Bug Report: STM32CubeMX 4.8.0 disallows selection of ADC1 channels Vbat or temperature

philip239955
Associate
Posted on June 17, 2015 at 01:17

I can't select ADC1 channels Vbat and temperature sensor at the same time. The reference manual mentions a restriction where those channels cannot be selected at the same time for the STM32F42x/STM32F43x in section 13.3.3, but it does not mention that restriction for the 40x/41x. I would expect them to both be selectable for my STM32F405, as they are on different channels (18 and 16, respectively).

0690X00000605gfQAA.png

#stm32cubemx
1 REPLY 1
Amel NASRI
ST Employee
Posted on June 17, 2015 at 15:01

Hello Philip,

I confirm this issue with CubeMX when using STM32F405/407/415/417.

Thanks for reporting, it will be fixed in coming release.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.