cancel
Showing results for 
Search instead for 
Did you mean: 

BUG: CubeMX doesn't mark IOC 'changed' when pin function or user-label changed

Editing an IOC in CubeMX IDE and using Pin & Configuration view, changing a pin's special-function or user label does not mark the IOC as changed. Consequently File Save remains grayed-out and it is not possible to save the changes.

@Markus GIRDLAND​ - Please confirm you can reproduce this and a ticket has been opened, Thanks!

Best Regards, Dave

PS: IOC attached illustrates the problem.

STM32CubeIDE, Version: 1.0.2, Build: 3566_20190716-0927

Try changing pin PA4

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Thanks @Markus GIRDLAND​ - Windows 10 Pro.

Now I can't reproduce it either. Restarted IDE and it works now.

Two oddities possibly related but...

1) I did Windows sleep/resume cycle after last save and before it got into this state

2) The clock calculation is quite deranged after I disabled PH1 (clock is externally generated so PH1 is not used for OSC-OUT function)

Aaarrrgggg.....

View solution in original post

4 REPLIES 4
Pavel A.
Super User

Which Cube version and which pins? CubeMX or CubeIDE?

Cannot reproduce here with STM32CubeMX 5.3.0 on Ubuntu.

-- pa

@Pavel A.​ - Thanks, I clarified the question.

Markus GIRDLAND
ST Employee

I can't reproduce this either. What is PA4 currently and what are you changing it to in your tests?

What OS are you using?

Thanks @Markus GIRDLAND​ - Windows 10 Pro.

Now I can't reproduce it either. Restarted IDE and it works now.

Two oddities possibly related but...

1) I did Windows sleep/resume cycle after last save and before it got into this state

2) The clock calculation is quite deranged after I disabled PH1 (clock is externally generated so PH1 is not used for OSC-OUT function)

Aaarrrgggg.....