cancel
Showing results for 
Search instead for 
Did you mean: 

BUG: CubeMX/CubeIDE does not initialize TIM20.TRGO2 on STM32G474.

Herm
Associate III

The configuration for the Timer 20 TRGO2 setting is not included in the generated source code. I verified using "git diff" that when changing the setting the only modified file is the .ioc.

I'm using the low level library for this timer. I haven't verifed if it happens with HAL as well.

CubeIDE:

Version: 1.2.1

Build: 5190_20200115_1224 (UTC)

STM32CubeG4 Firmware Package V1.1.0 / 28-June-2019

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Khouloud ZEMMELI
ST Employee

​Hello @Herm​ ,

Thanks for your feedback, issue appears only with LL, it works fine with HAL.

It will be fixed in the next release.

Best Regards,

Khouloud

View solution in original post

1 REPLY 1
Khouloud ZEMMELI
ST Employee

​Hello @Herm​ ,

Thanks for your feedback, issue appears only with LL, it works fine with HAL.

It will be fixed in the next release.

Best Regards,

Khouloud