cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 6.15.0 unnecessarily configures R1 pin in LTDC peripheral when using RGB666 Display

Craig_Robertson
Visitor

For the STM32H743IIKx micro, CubeMX 6.15.0 unnecessarily creates a configuration for the R1 pin when creating an LTDC peripheral when using the RGB666 Display Type.

This should not be configured. The required R* pins for this Display Type are R2-R7, as per G2-G7 and B2-B7.

This did not occur in previous CubeMX versions, including 6.14.1.

This bug means that it is not possible to upgrade to this version of CubeMX with an existing project that already uses the pin(s) required for LTDC_R1. 

2 REPLIES 2
Mahmoud Ben Romdhane
ST Employee

Hello @Craig_Robertson ,

 

First let me thank you for posting and welcome to the ST Community.

Your request is under investigation, and I will get back to you ASAP.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Mahmoud Ben Romdhane
ST Employee

Hello @Craig_Robertson ,

 

It is a regression on the STM32CubeMX V6.15.0.

This is a known Issue, and an internal Ticket was submitted to the Development Team 

(Internal Ticket Number: 215387).

I will keep you up to date when the problem is solved.

 

Best Regards.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.