2023-10-12 12:55 AM
Hello,
When I add a .bat script to:
Project-Manager -> Code Generator -> User Actions -> Before/After code generation
I figure out that CubeMX freezes when the Outputs window is disabled.
It is especially problematic when launching a CubeMx script.
Do you know where it comes from? And how to avoid this undesirable behavior?
Thank you for your answer
PS: Is it possible to run scripts other than .bat files ?
2023-10-17 06:21 AM - edited 2023-10-17 06:46 AM
Hello @dletinaud
And welcome to the community!
Could you please provide more information about the version of CubeMX ,the MCU and the .bat file you use.
Thank you
Souhaib
2023-10-20 01:23 AM
Hi @Souhaib MAZHOUD,
I tested it with the version 6.9.2.
I tested it with multiple .bat scripts, the last ones were just an echo or writing a string to a file. They worked well when launched manually.
Script name had no special characters, it was named "patch.bat".
2023-11-08 05:43 AM
Hello @Souhaib MAZHOUD,
The project was for a STM32F745VGT6.
Do you have any information for this bug ?
Did I make a mistake ? Do you succeed to repeat the bug ?
Can it be reported to the dev team ?
Thanks for your response
David
2023-11-08 06:54 AM - edited 2023-11-08 06:58 AM
> CubeMX freezes when the Outputs window is disabled.
@dletinaud If the Outputs window is shown, the problem won't occur?
#bugreport
2023-11-08 06:55 AM
Yes indeed
2023-11-09 12:42 AM
Hello @dletinaud,
Actually, the issue has been escalated to the dev team and is currently under investigation.
Internal ticket number: 164200 (This is an internal tracking number and is not accessible or usable by customers).
Thank you,
Souhaib
2023-11-09 02:22 AM
Hello @Souhaib MAZHOUD,
Thank you for your reply and your support