B-L475e-IOT Board USB CDC not working / recognized
Dear all,
I am struggling with the B-L475e-IOT board and USB. If I use the default initialisation of CubeMX and change the USB device to OTG FS Device only and add the Middleware of the Communication device class I can not get this as recognized device on Win 7 as well as Win 10.
The line coding is set within usbd_cdc_if.c as in the USB mooc as follows in CDC_Control_FS and Linecoding is defined and initialized as follows:
USBD_CDC_LineCodingTypeDef Linecoding = {
115200, /*baudrate*/
0x00, /*stop bits-1*/
0x00, /*parity none*/
0x08, /*no of bits*/}; case CDC_SET_LINE_CODING:
Linecoding.bitrate = (uint32_t)(pbuf[0] | pbuf[1] << 8 |\
pbuf[2] << 16 | pbuf[3] << 24);
Linecoding.format = pbuf[4];
Linecoding.paritytype = pbuf[5];
Linecoding.datatype = pbuf[6];
break;
case CDC_GET_LINE_CODING:
pbuf[0] = (uint8_t)(Linecoding.bitrate);
pbuf[1] = (uint8_t)(Linecoding.bitrate>>8);
pbuf[2] = (uint8_t)(Linecoding.bitrate>>16);
pbuf[3] = (uint8_t)(Linecoding.bitrate>>24);
pbuf[4] = Linecoding.format;
pbuf[5] = Linecoding.paritytype;
pbuf[6] = Linecoding.datatype;
break;Using other STMs I got it working the same way. Is there any obvious thing which I do not see for now? With the other controllers I can even see them in device manager as Com Port right after the execution of MX_USB_DEVICE_Init(). Here I only get an unknown device.
Hopefully someone sees what the issue is, thanks in advance,
Marcel