cancel
Showing results for 
Search instead for 
Did you mean: 

Availability of I-Cube-CANOPEN package from Emotas on a STM32F7

CObri.1
Associate III

I would like to use the CAN interface with a CANOPEN library on my STM32F723.

As I have found there is a Library for STM chips provided by emotas: https://www.st.com/en/partner-products-and-services/canopen.html

I have downloaded the Lib on my STM32CubeIDE an now are trying to add it in my CubeMX to the Project:

CObri1_0-1736959621624.png

The problem is, it says, its not supporting my MCU. But in the description of the Library it says it should support the F7 chips.

Is the library not "free" and I have first to contact emotas or did I forget to install something?

Best regards,
CO

4 REPLIES 4
mƎALLEm
ST Employee

Hello,

I'm checking internally and get back to you as soon as I have a feedback.

Just note that the Emotas stuck is provided as an evaluation version and for commercial usage need to contact them directly.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Are there any news about this ticket?
Best regards,
CO

I'm still waiting for an answer.

I will get back to you as soon as I have a feedback.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
mƎALLEm
ST Employee

Hello,

I'm getting back to you with the answer.

In fact there are two offers for emotas CANOpen:

1- This link

mALLEm_0-1740992860724.png

This offer is for commercial usage and you need to contact emotas over their website: https://www.emotas.de/en/contact

2 This link: which corresponds to I-CUBE-CANOPEN package.

mALLEm_1-1740993023765.png

This package is only for evaluation and (for the moment) supports only these MCUs:

From the release notes: Middlewares\Third_Party\emotas_CANopen\emotas\Release_Notes.html

mALLEm_2-1740993216027.png

We only put the supported devices STM32G4 in our webpage because it was the only platform validated from our side. 

So indeed I-CUBE-CANOPEN does not support STM32F7 family. You need to contact Emotas for that device (the first offer).

Hope that answers your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.