cancel
Showing results for 
Search instead for 
Did you mean: 

Support for J-Link and J-Link OB?

Hueli.1
Associate III

In the hardware requirements for the STM32CubeMonitor it is mentioned that an “STM32 target board“ is required. (wiki)

Does that mean that the monitor is not compatible with J-Link and J-Link OB and for example an STM32L433CC ?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
stephane.legargeant
ST Employee

Hello

J-Link and J-Link OB are not supported by STM32CubeMonitor. Version 1.0.0 supports only ST-Link probes (or boards including ST-Link like Nucleo).

Best regards

Stephane

View solution in original post

8 REPLIES 8
stephane.legargeant
ST Employee

Hello

J-Link and J-Link OB are not supported by STM32CubeMonitor. Version 1.0.0 supports only ST-Link probes (or boards including ST-Link like Nucleo).

Best regards

Stephane

WToth
Associate

Any plans to support J-Link in the future?

Hello

There is no plan to support this probes right now.

Best regards

Stephane

That's such a pity. J-Link is such a popular probe and having to switch between an ST-Link and J-Link to use this application is just extra hassle. Could you not contact Segger and ask for assistance in adding support?

Up

Up from my side also..

VYERS.1
Associate
  • I join the question

Upvote