2022-11-13 5:59 PM
This is a serial input, the data volume per second is 12000bytes (1k Sampling rate*4channel*3bytes (single-channel sampling data size)). The input content of the serial port is as follows (part of the picture is intercepted) :serial port output format: 3 bytes data + 'comma'
The procedure is as follows:
2022-11-13 6:05 PM
The code is to long, I can't insert it.