2020-04-20 4:13 AM
I think this page would have the content:
https://wiki.st.com/stm32mcu/wiki/STM32CubeMonitor:How_to_write_a_variable_from_flow
It seems that hashKey value can not be read out somewhere?
{"variablelist":[{"address":"{{flow.current_limit_adr}}","name":"current_limit","type":5,"checked":true,"$$hashKey":"object:604","value":"{{payload}}","validity":true}],"accesspoint":0}
(I know how to use the write panel - but need to set 1 variable with value from flow)
Solved! Go to Solution.
2020-04-20 4:52 AM
Hello
To write data by flow, the following payload must be sent to probe out node ,with the topic “write�? :
{
"variablelist": [
{
"address": "0x20000060",
"type": 4,
"value": "xxxx"
}
],
"accesspoint": 0
}
The question has been asked in this topic : https://community.st.com/s/question/0D53W000000ayg1SAA/hello-how-is-it-possible-to-change-a-variable-by-pressing-a-buttoni-just-can-change-a-variable-by-using-the-write-panel-butregards
The post explains with details how to write variable from the flow without using the write-panel. It should answer you point.
We are preparing a wiki page, but it is not finalized yet. So there is just a placeholder right now on the wiki.
best regards
Stephane
2020-04-20 4:52 AM
Hello
To write data by flow, the following payload must be sent to probe out node ,with the topic “write�? :
{
"variablelist": [
{
"address": "0x20000060",
"type": 4,
"value": "xxxx"
}
],
"accesspoint": 0
}
The question has been asked in this topic : https://community.st.com/s/question/0D53W000000ayg1SAA/hello-how-is-it-possible-to-change-a-variable-by-pressing-a-buttoni-just-can-change-a-variable-by-using-the-write-panel-butregards
The post explains with details how to write variable from the flow without using the write-panel. It should answer you point.
We are preparing a wiki page, but it is not finalized yet. So there is just a placeholder right now on the wiki.
best regards
Stephane
2020-04-20 5:10 AM
Thanks.... I only forgot the "write" topic :(
"$$hashKey":"object:604"
"validity":true
These 2 is for no use?
/Kasper
2020-04-20 5:44 AM
You don't need to take care of "$$hashKey" and "validity" to write from flow.
Stephane
2020-04-20 5:48 AM
Got it - and stuff is working.
This is really a good and powerfull tool you have produced here - Thank you!!
Just as a feedback, i had some problems with adding 2 variables blocks to select different variables, then it uses the same exe config, and mixes up the variables between them.... i ended up using only one variables block and manual parse them out.
On the other hand i could have made several variabel blocks, and connect direct to chart.
/Kasper
2021-11-11 2:10 PM
Hello,
I follow the instruction and i receive this error:
"Bad parameter (7)"
msg : string[264]
"Unsuccessful write (Bad parameter (7)) on 48FF6E064986484820270787, for data = "{\n \"variablelist\": [\n {\n \"address\": \"0x20000000\",\n \"type\": 3,\n \"value\": \"3678\"\n }\n ],\n \"accesspoint\": 0\n}": write"
Do you know what's wrong with it? I check the address and i type and they are correct.
2021-11-15 10:03 AM
Hello
I thing the \n in the log are strange.
Can you compare with the wiki example here : STM32CubeMonitor:How to write a variable from flow - stm32mcu ?
Take care to set the output of "template" node to "parsed JSON".
If not ok, can you insert a debug node after "set topic" node to see what is sent to the node "myProbe_Out" ?
Please let us know the result.
Best regards
Stephane
2021-11-15 1:54 PM
Hello,
I do the same work as the link, this is my basic flow .
thank you
2021-11-16 3:20 AM
Do you mean that it is still not working ?
If it is not working, could you share your flow with me ? (at least export the nodes on the top part)
Best regards
Stephane
2021-11-17 2:21 AM