2022-11-21 07:52 AM
I want to get mass data and display all these data on STM-Studio without delay.
but, Using default setting [acquisition rate is Maximum, Select "Display all data"] ,
I can get and display mass data with delay.
To get/display mass data without delay, Waht do you recomend for me ?
Are these charanges good idea ?
please hint for me.
thank you.
Solved! Go to Solution.
2022-11-25 07:37 AM
Hi @Community member ,
New solution to replace STM-Studio is STM32CubeMonitor.
Some of the offered features:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-11-21 11:51 AM
Perhaps architect a solution using USB directly (STM32 to PC) that off-boards the volume of data you have?
2022-11-21 08:36 PM
Thank you for replying.
I can't use USB peripheral in my project.....
but , that is good idea.
Do you have the others idea ?
2022-11-25 07:37 AM
Hi @Community member ,
New solution to replace STM-Studio is STM32CubeMonitor.
Some of the offered features:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.