STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

Resolved! Simple Led Blink with STM32CubeMonitor

Hello Everyone,Sorry if this is a stupid question.I just found this software STM32CubeMonitor and as a starting point I started with a simple LED Blink Example.In my example there are two variables "led_green_state" and "led_red_state" and the value ...

Resolved! How to layout dashboard components as a whole

Dear all,How to adjust the layout of dashboard components as a whole?I now find that each component can only be individually sized and cannot be placed in a single panel to evaluate the layout as a whole.My dashboard is a mess.

0693W000003C2EQQA0.png
Fhu.1 by Associate II
  • 1681 Views
  • 2 replies
  • 0 kudos

Resolved! realtime variable edit without cube monitor

​I'm using Keil IDE to program stm32 microcontrollers, Keil IDE allows to change variable's value "while code running" without breakpoints.​I want to use Cubeide instead Keil.​I can use live expression tool for watching values "while code running" bu...

Oanar.1 by Associate
  • 1664 Views
  • 3 replies
  • 0 kudos

Resolved! filter or routing variables to UI

Hello, I think it is a basic question but I can't find a solution.I read 4 variables, 2 fan RPM and 2 temperatures.I route the two RPM to a gauge, and I would like the temperature to a char (only the temperature). Because the scale is very different...

0693W000001t5BmQAI.png
PCu1 by Senior
  • 1314 Views
  • 2 replies
  • 0 kudos

Resolved! Variable node configuration lost after build

Hi everyone,I have been using STM32CubeMonitor for some time and I love this tool. The only problem I have is when I compile my code, I have to reselect the variables in the configuration of the variable nodes. Is there a way for the software to reme...

AViau.1 by Associate
  • 1297 Views
  • 1 replies
  • 0 kudos