Application server port already in use
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-03-09 10:07 AM
When starting STM32CubeMonitor it displays a dialog reporting "Application server port already in use"; the application then exits when the dialog is closed.
In the details it says that port 1880 is already in use; however netstat doesn't show this port as being used. (Windows 10, 64-bit).
Any suggestions?
Thanks,
Simon
Solved! Go to Solution.
- Labels:
-
STM32CubeMonitor
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-10 9:33 AM
Just a quick note to help.
I had exactly the same issue and tracked it down to a bug to STM32CubeMonitor. The ST software basically try to communicate with the wrong network interface. Disabling Hyper-V didn't help here, because I also have VMware installed and it causes the same issue.
To fix it, you have to disable all virtual network interface in Control Panel\All Control Panel Items\Network Connections
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-03-09 10:54 AM
Hello
Usually, this happens when STM32CubeMonitor is already running. As the port 1880 is already busy, the second instance closes after the warning.
Have you tried netstat -a ? (On my PC, netstat does not show locals connections)
Best regards
Stephane
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-03-09 12:26 PM
Hi Stephane, thanks for your reply.
STM32CubeMonitor is not already running; it has just been installed, I've not been able to run it even once. The PC has been rebooted; the issue is the same afterwards. I have tried various netstat options (including the '-a' you suggested); there is no indication that port 1880 is in use as far as I can see.
Thanks,
Simon
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-03-10 6:39 AM
An update; the following command shows ports which are being excluded:
> netsh int ip show excludedportrange protocol=tcp
Protocol tcp Port Exclusion Ranges
Start Port End Port
---------- --------
1827 1926
1927 2026
2027 2126
2180 2279
2280 2379
2456 2555
2869 2869
3029 3128
3719 3818
5357 5357
5700 5700
8884 8884
8888 8888
50000 50059 *
* - Administered port exclusions.
This was due to 'Hyper-V' - by disabling Hyper-V I have been able to start STM32CubeMonitor sucessfully.
Kind regards,
Simon
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-03-10 8:51 AM
Hello Simon
Thanks a lot for your feedback. It is useful information for people using Hyper-V or similar software.
Stephane
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-10 9:33 AM
Just a quick note to help.
I had exactly the same issue and tracked it down to a bug to STM32CubeMonitor. The ST software basically try to communicate with the wrong network interface. Disabling Hyper-V didn't help here, because I also have VMware installed and it causes the same issue.
To fix it, you have to disable all virtual network interface in Control Panel\All Control Panel Items\Network Connections